Write/Read
About Auto Port Extensions

AutoPortExtLoss Property


Description

Specifies whether or not to include loss correction as part of automatic port extension. Learn more about Loss Compensation in port extension.

 VB Syntax

fixture.AutoPortExtLoss = bool

Variable

(Type) - Description

fixture

A Fixturing (object)

bool

True - Includes Loss correction.

False - Does NOT include Loss correction.

Return Type

Boolean

Default

False

Examples

fixture.AutoPortExtLoss = True

value = fixture.AutoPortExtLoss 'Read

C++ Syntax

HRESULT get_AutoPortExtLoss(VARIANT_BOOL *pState);

HRESULT put_AutoPortExtLoss(VARIANT_BOOL bState);

Interface

IFixturing2