Read-only |
About Auxiliary Triggering |
Description |
Returns the number of aux trigger input / output connector pairs in the PNA |
VB Syntax |
value = app.AuxiliaryTriggerCount |
Variable |
(Type) - Description |
|
value |
(Long Integer) Variable to store the returned value. 2 = PNA-X models 1 = All other PNA models |
|
app |
An Application (object) |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
ioConns = app.AuxiliaryTriggerCount |
C++ Syntax |
HRESULT AuxiliaryTriggerCount(long *count); |
Interface |
IApplication11 |