Write/Read
About Balanced Measurements

BalancedMode Property


Description

Sets and returns whether the balanced transform is ON or OFF

 VB Syntax

balMeas.BalancedMode = value

Variable

(Type) - Description

balMeas

A BalancedMeasurement (object)

value

(Boolean) - State of balanced transform. Choose from

False  Balanced Transform OFF

True  Balanced Transform ON

Return Type

Boolean

Default

False

Examples

balMeas.BalancedMode = True 'Write

variable = balMeas.BalancedMode  'Read

C++ Syntax

HRESULT get_BalancedMode(VARIANT_BOOL *bVal)

HRESULT put_BalancedMode(VARIANT_BOOL newVal)

Interface

IBalancedMeasurement