Read only

 

CalibrationName  Property


Description

Returns the name of the current Cal Type.

 VB Syntax

value = meas.CalibrationName

Variable

(Type) - Description

value

(string) - Variable to store the returned value.

meas

A Measurement  (object)

Return Type

String

Default

Not Applicable

Examples

ct = meas.CalibrationName

C++ Syntax

HRESULT get_CalibrationName( BSTR* CalibrationName);

Interface

IMeasurement2