Read / Write |
About User Characterization |
Description |
Sets or queries the connector type for the specified port. |
VB Syntax |
ecalUser.ConnectorType (port) = value |
Variable |
(Type) - Description |
ecalUser |
An ECalUserCharacterizer (object) |
port |
(Enum) ECal port for which connector type is to be set. Choose from: 1 or naECalPort_A 2 or naECalPort_B 3 or naECalPort_C 4 or naECalPort_D |
value |
(String) - Connector type. When the User Characterization is to be stored in the ECal module, then the connector type is limited to a Factory-defined connector type. See the list. When the User Characterization is to be stored in PNA disk memory, then the connector type can also be a User-defined connector type. |
Return Type |
String |
Default |
"" (Empty String) |
Examples |
ecalUser.ConnectorType(naECalPort_B) = "APC 3.5 male" ' Write |
Value = ecalUser.ConnectorType(naECalPort_B) |
|
C++ Syntax |
HRESULT get_ConnectorType(NAECalPort port, BSTR *connector); HRESULT put_ConnectorType(NAECalPort port, BSTR connector); |
Interface |
IECalUserCharacterizer |