Write/Read |
About E5091 Testset ControlAbout External Testset Control |
Description |
Sets the control lines of the specified test set. Control lines, provided through the front panel connector of a test set, are used to control external equipment such as a part handler. See your test set documentation to learn more about control lines. |
||||||||||||||||||
VB Syntax |
tset.ControlLines (chNum) = value |
||||||||||||||||||
Variable |
(Type) - Description |
||||||||||||||||||
|
tset |
A TestsetControl object. OR An E5091Testset object. |
||||||||||||||||||
|
chNum |
(Integer) Channel number of the measurement. |
||||||||||||||||||
|
value |
(Double) Data value used to set control lines. Values are obtained by adding weights from the following table that correspond to individual lines.
Refer to your test set documentation for setting control line values. |
||||||||||||||||||
Return Type |
Variant |
||||||||||||||||||
Default |
0 |
||||||||||||||||||
Examples |
'For a Z5623A K64 test set, the following sets line 3 and 4 OFF; all other lines ON. testset1.ControlLines(2) = 12 |
||||||||||||||||||
C++ Syntax |
HRESULT get_ControlLines(long channelNum, VARIANT *stateByte); |
||||||||||||||||||
Interface |
ITestsetControl IE5091Testset |