Write/Read | 
About Power Coupling | 
Description | 
 Turns ON and OFF port power coupling. ON means the power level is the same for both ports. OFF means the power level may be set independently for each port.  | 
VB Syntax | 
 object.CouplePorts = value  | 
Variable | 
(Type) - Description | 
| 
 object  | 
 Channel (object) or CalSet (object) - Read-only property  | 
| 
 value  | 
 (enum NAStates) Choose from: 0 - NaOff - Turns coupling OFF 1 - NaOn - Turns coupling ON  | 
Return Type | 
 Long Integer  | 
Default | 
 NaON (1)  | 
Examples | 
 chan.CouplePorts = NaOff 'Write  | 
| 
 couplport = chan.CouplePorts 'Read  | 
|
C++ Syntax | 
 HRESULT get_CouplePorts(tagNAStates *pState)  | 
Interface | 
 IChannel |CalSet3  |