Write/Read
About Time Domain Trace Coupling

CoupledParameters Property (Gating)


Description

Specifies the time domain gating parameters to be coupled. The settings for those parameters will be copied from the active measurement to all other measurements on the channel.

To turn coupling ON and OFF, use CoupleChannelParams Property

To specify Transform parameters to couple, use Transform.CoupledParameters Property

 VB Syntax

gate.CoupledParameters = value

Variable

(Type) - Description

trans

A Gating (object)

value

(Enum As NAGatingCoupledParams) - Parameters to couple. To specify more than one parameter, add the numbers. Choose from:

1 - naGatingStimulusCoupled (Start, Stop, Center, and Span TIME settings.)

2 - naGateStateCoupled (ON / OFF)

4 - naGatingShapeCoupled (Minimum, Normal, Wide, and Maximum)

8 - naGatingTypeCoupled (Bandpass and Notch)

Return Type

Enum

Default

29

Examples

gate.CoupledParameters = 15 'Couple all parameters

CP = gate.CoupledParameters 'Read

C++ Syntax

HRESULT get_CoupledParameters(long *lParams);

HRESULT put_CoupledParameters(long lParams);

Interface

IGating2