Read-only
 

CustomMeasurementConfiguration Property


Description

Returns a handle to a custom measurement object on the active channel. You can use the handle to access custom measurement properties and methods.

Currently, the custom measurement objects to which this property provides access is:

 VB Syntax

Set custMeas = meas.CustomMeasurementConfiguration

Variable

(Type) - Description

custMeas

A variable in which the handle to a custom measurement is returned. (object)

chan

A Measurement (object)

Return Type

Custom Measurement object

Default

None

Examples

See examples:GainCompression

C++ Syntax

HRESULT CustomMeasurementConfiguration(IDispatch** value);

Interface

IMeaurement12