Write/Read
 

DCState Property


Description

Set and read the specified DC source’s ON/OFF state in the multi-dimensional sweep.

 VB Syntax

md.DCState (name,port) = value

Variable

(Type) - Description

md

A MultiDimensionalSweep (object) which belongs to a SA channel.

name,port

(string) Name of the "DC source, port"

value

(Boolean) Choose from:

0 - OFF -Disable the specified DC source in multi-dimensional sweep.

1 - ON - Enable the specified DC source in multi-dimensional sweep.

Return Type

Boolean

Default

0

Examples

md.DCState ("AO1") = OFF   'Write

value = md.DCState("MyDCSource,Port 1") 'Read

C++ Syntax

HRESULT put_DCState (BSTR name, VARIANT_BOOL value);

HRESULT get_DCState (BSTR name, VARIANT_BOOL* value);

Interface

IMultiDimensionalSweep