Read-only

ECALCharacterizationIndexList Property


Description

Returns a list of characterizations stored in the specified ECal module.  Learn more about ECal User characterization.

 VB Syntax

clist = cal.ECALCharacterizationIndexList (moduleNum)

Variable

(Type) - Description

clist

Variable to store the returned list of characterization index numbers.

cal

Calibrator (object)

module

ECal module from which to read user characterization numbers.

Return Type

Variant

Default

Not Applicable

Examples

'Module 1 contains User Characterizations 1 and 3.
clist = cal.ECALCharacterizationIndexList(1)

'Returns the following (0 always indicates the factory characterization):
0,1,3

C++ Syntax

HRESULT get_ECALCharacterizationIndexList( long moduleNumber, VARIANT *characterizations);

Interface

ICalibrator6