Write / Read
About ECal User Characterization

ECalID Property


Description

Selects the model and serial number of the ECal module to be characterized. This command does NOT set the model and serial number of the ECal module.

 VB Syntax

userChar.ECalID = value

Variable

(Type) - Description

userChar

An ECalUserCharacterizer Object

value

(String) Model and serial number of the ECal module to be characterized.

Return Type

String

Default

"" (Empty String)

Examples

userChar.ECalID ="N4433A,00001"

C++ Syntax

HRESULT put_ECalID(BSTR id);

Interface

IECalUserCharacterizer