Write/Read
About Electrical Delay

ElectricalDelay Property


Description

Sets the Electrical Delay for the active channel.

 VB Syntax

meas.ElectricalDelay = value

Variable

(Type) - Description

meas

A Measurement (object)

value

(double) - Electrical Delay in seconds. Choose any number between -9.99 and 9.99

Return Type

Double

Default

0

Examples

meas.ElectricalDelay = 1e-3 'Write

edelay = meas.ElectricalDelay 'Read

C++ Syntax

HRESULT get_ElectricalDelay(double *pVal)
HRESULT put_ElectricalDelay(double newVal)

Interface

IMeasurement