Write/Read |
About ExternalDevices |
Description |
Set and return whether External Devices remain activated or are de-activated when the PNA is Preset or when a Instrument State is recalled. This setting remains until changed again using this command, or until the hard drive is changed or reformatted. See the ExternalDevices collection. |
VB Syntax |
pref.ExternalDeviceDeActivatePolicy = value |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
value |
(Boolean) - Choose from:
|
Return Type |
Boolean |
Default |
True |
Examples |
pref.ExternalDeviceDeActivatePolicy = 1 'Write |
|
dDevPolicy = pref.ExternalDeviceDeActivatePolicy 'Read |
|
C++ Syntax |
HRESULT get_ExternalDeviceDeActivatePolicy(VARIANT_BOOL * pref); HRESULT put_ExternalDeviceDeActivatePolicy(VARIANT_BOOL pref); |
Interface |
IPreferences10 |