Write/Read |
About Frequency Offset |
Description |
This method is replaced by properties on the FOMRange Object. Establishes a fixed (CW) stimulus frequency while measuring the Response over a swept frequency range. For example, a fixed-frequency PNA stimulus may be applied to the RF input of a mixer whose local oscillator (LO) is being swept. Because the IF output of the mixer will be swept, the PNA receivers must also be swept. See other Frequency Offset properties. |
VB Syntax |
object.FrequencyOffsetCWOverride = value |
Variable |
(Type) - Description |
|
object |
Channel (object) or CalSet (object) - Read-only property |
|
value |
(Enum as NaStates) - Choose from: naOFF (0) - Turns CW override OFF naON (1) - Turns CW override ON |
Return Type |
Enum |
Default |
0 Hz |
Examples |
chan.FrequencyOffsetCWOverride = 1 'Write |
|
fOffsetOV = chan.FrequencyOffsetCWOverride 'Read |
|
C++ Syntax |
HRESULT get_FrequencyOffsetCWOverride (tagNAStates *pstate) |
Interface |
IChannel2 |CalSet3 |