Write/Read
About Frequency Offset

FrequencyOffsetFrequency Property  Superseded


Description

This method is replaced by properties on the FOMRange Object.

Specifies an absolute offset frequency in Hz. For mixer measurements, this would be the LO frequency. See other Frequency Offset properties.

 VB Syntax

object.FrequencyOffsetFrequency  = value

Variable

(Type) - Description

object

Channel (object)

or

CalSet (object) - Read-only property

value

(Double) - Offset value. Range is +/- 1000 GHz.  (Offsets can be positive or negative.)

Return Type

Double

Default

0 Hz

Examples

chan.FrequencyOffsetFrequency = 2 'Write

fOffsetFreq = chan.FrequencyOffsetFrequency 'Read

C++ Syntax

HRESULT get_FrequencyOffsetFrequency(double*pval)
HRESULT put_FrequencyOffsetFrequency(double newVal)

Interface

IChannel2

|CalSet3