Write/Read
About Frequency Offset

FrequencyOffsetState Property  Superseded


Description

This method is replaced by properties on the FOMRange Object.

Enables Frequency Offset on ALL measurements that are present on the active channel. This immediately causes the source and receiver to tune to separate frequencies. The receiver frequencies are specified with other channel and offset settings. To make the stimulus settings, use Channel Start, Stop Frequency properties.  See other Frequency Offset properties.

Tip: To avoid unnecessary errors, first make other frequency offset settings. Then turn Frequency Offset ON.

 VB Syntax

object.FrequencyOffsetState  = value

Variable

(Type) - Description

object

Channel (object)

or

CalSet (object) - Read-only property

value

(Enum as NaStates) - Choose from:

naOFF (0) - Turns Frequency Offset OFF

naON (1) - Turns Frequency Offset ON

Return Type

Enum

Default

naOFF (0)

Examples

chan.FrequencyOffsetState = naON 'Write

Foffset = chan.FrequencyOffsetState 'Read

C++ Syntax

HRESULT FrequencyOffsetState (tag NAStates *pState);
HRESULT FrequencyOffsetState (tag NAStates newState)

Interface

IChannel2

|CalSet3