Write/Read |
About Receiver Leveling |
Description |
Sets and returns the frequency range to use for receiver leveling. On the user interface, this is the "Receiver frequency is determined by:" setting. |
VB Syntax |
RxLevel.FrequencyType(srcPort) = value |
Variable |
(Type) - Description |
|
RxLevel |
A ReceiverLeveling Object |
|
srcPort |
(Long Integer) Source port for Receiver Leveling. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(Enum) Frequency range. Choose from: naAutoFrequency (0) - always uses the frequency range that is assigned to the measurement receiver. naInputFrequency (3) - Mixer/Converter input frequency range. naOutputFrequency (4) - Mixer/Converter input frequency range. naReceiverFrequency (1) - FOM Receiver frequency range. naSourceFrequency (2) - FOM Source frequency range |
Return Type |
Enum |
Default |
naAutoFrequency (0) |
Examples |
rxLevel.FrequencyType (1) = naAutoFrequency ' Write |
|
value = rxLevel.FrequencyType 2' Read |
|
C++ Syntax |
HRESULT get_FrequencyType(long port, tagNAFrequencyType* pVal); HRESULT put_FrequencyType(long port, tagNAFrequencyType newVal); |
Interface |
IRxLevelingConfiguration3 |
Last Modified:
|
8-Mar-2012 |
MX New topic |