Write/Read |
About GPIB Fundamentals |
Description |
Changes the analyzer to a GPIB system controller or a talker/listener on the bus. The analyzer must be the controller if you want to use it to send commands to other instruments. The analyzer must be a talker/listener if you want to send it commands from another PC. Note: This command has no affect in PNAs with dedicated Controller and Talker/Listener GPIB connectors. |
VB Syntax |
app.GPIBMode value |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
value |
(enum NAGPIBMode) -Choose either: |
Return Type |
Long Integer |
Default |
0 - naTalkerListener |
Examples |
app.GPIBMode = naTalkerListener 'Write |
|
mode = app.GPIBMode 'Read |
|
C++ Syntax |
HRESULT get_GPIBMode(tagGPIBModeEnum* eGpibMode) |
Interface |
IApplication |