Read-only

IDString Property


Description

Returns the ID of the analyzer, including the Model number, Serial Number, and the Software revision number.

Note: Beginning with Rev 6.01, this command now returns the software revision with 6 digits instead of 4. For example, A.06.01.02.

 VB Syntax

value = app.IDString

Variable

(Type) - Description

app

An Application (object)

value

(string) - variable to contain the returned ID string

Return Type

String

Default

Not Applicable

Examples

id = app.IDString

C++ Syntax

HRESULT IDString(BSTR* IDString)

Interface

IApplication