Write/Read
About Time Domain

ImpulseWidth Property


Description

Sets or returns the Impulse Width of Time Domain transform windows

 VB Syntax

trans.ImpulseWidth = value

Variable

(Type) - Description

trans

A Transform (object)

value

(double) - Impulse Width in seconds. Range of settings depends on the frequency range of your analyzer.

Return Type

Double

Default

.98 / Default Span

Examples

trans.ImpulseWidth = 200e-12 'sets the Impulse width of a transform window -Write

IW = trans.ImpulseWidth 'Read

C++ Syntax

HRESULT get_ImpulseWidth(double *pVal)
HRESULT put_ImpulseWidth(double newVal)

Interface

ITransform