Write/Read
About SMC CalTypes

IncludeReverseSweep Property


Description

Sets whether to include SC12 sweeps during measurements.

 VB Syntax

obj.IncludeReverseSweep = bool

Variable

(Type) - Description

obj

A Converter (object)

bool

(Boolean) -

True - Include the SC12 (reverse) sweep.

False - Do NOT Include the SC12 (reverse) sweep.

Return Type

Boolean

Default

True

Examples

obj.IncludeReverseSweep = True

C++ Syntax

HRESULT get_IncludeReverseSweep(VARIANT_BOOL * val);

HRESULT put_IncludeReverseSweep(VARIANT_BOOL val);

Interface

IMixer12