Write/Read

Invert Property


Description

Sets whether to invert the polarity of the pulse.

 VB Syntax

pulse.Invert (n) = value

Variable

(Type) - Description

pulse

A PulseGenerator (object)

n

(Integer) Pulse generator number. Choose from 0 to 4.

Or use PulseGeneratorID to refer to an external pulse generator.

0 is the generator that pulses the ADC.

value

True - Invert the pulse generator polarity. This causes the pulse ON time to be active low and OFF be active high.

False - Do NOT Invert the pulse generator polarity.

Return Type

Boolean

Default

False

Examples

pulse.Invert(1) = True 'Write

value = pulse.Invert(4) 'Read

C++ Syntax

HRESULT get_Invert(integer pulse, VARIANT_BOOL *pVal);

HRESULT put_Invert(integer pulse, VARIANT_BOOL newVal);

Interface

IPulseGenerator4