Read-only | 
About Trigger | 
Description | 
 Returns whether or not a channel is in continuous mode. To set the channel to continuous mode, use Continuous Method.  | 
VB Syntax | 
 value = chan.IsContinuous  | 
Variable | 
(Type) - Description | 
| 
 value  | 
 (boolean) - Choose either: False - Channel trigger is NOT set to continuous. True - Channel trigger IS set to continuous.  | 
| 
 chan  | 
 Channel (object)  | 
Return Type | 
 Boolean  | 
Default | 
 Not Applicable  | 
Examples | 
 trig = chan.IsContinuous 'Read  | 
C++ Syntax | 
 HRESULT get_IsContinuous ( VARIANT_BOOL *bContinuous);  | 
Interface | 
 IChannel4  | 
Last Modified:
| 
 13-Nov-2013  | 
 Fixed Channel rev.  |