Read-only

IsSParameter Property


Description

Returns true if measurement represents an S-Parameter

 VB Syntax

value = meas.IsSparameter

Variable

(Type) - Description

meas

A Measurement (object)

value

(Boolean)

True - measurement is an S-Parameter

False - measurement is NOT an S-Parameter

Return Type

Boolean

Default

True

Examples

print app.IsSparameter

C++ Syntax

HRESULT IsSparameter( [out, retval] VARIANT_BOOL * bVal);

Interface

IMeasurement2