Write/Read |
About Receiver Leveling |
Description |
Sets and returns the maximum leveling sweep iterations to be used in order to achieve the tolerance setting. |
VB Syntax |
RxLevel.IterationNumber(srcPort) = value |
Variable |
(Type) - Description |
|
RxLevel |
A ReceiverLeveling Object |
|
srcPort |
(Long Integer) Source port for which to set the IterationNumber for Receiver Leveling. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(Long Integer) Max iterations. Choose a value between 1 and 25. |
Return Type |
(Long Integer) |
Default |
5 |
Examples |
rxLevel.IterationNumber (1) = 10 ' Write |
|
value = rxLevel.IterationNumber 2' Read |
|
C++ Syntax |
HRESULT get_IterationNumber(long port, long* pVal); HRESULT put_IterationNumber(long port, long newVal); |
Interface |
IReceiverLevelingConfiguration |
Last Modified:
|
13-Feb-2009 |
MX New topic |