Write/Read
About Time Domain

KaiserBeta Property


Description

Sets or returns the Kaiser Beta of Time Domain transform windows

 VB Syntax

trans.KaiserBeta = value

Variable

(Type) - Description

trans

A Transform (object)

value

(single) - Kaiser Beta. Choose any number between 0 and 13.

Return Type

Single

Default

0

Examples

trans.KaiserBeta = 6 'sets the Kaiser Beta of a transform window -Write

KB = trans.KaiserBeta 'Read

C++ Syntax

HRESULT get_KaiserBeta(float *pVal)
HRESULT put_KaiserBeta(float newVal)

Interface

ITransform