Write/Read |
About PMAR |
Description |
Enable or disable the use of the power meter min and max frequencies. |
VB Syntax |
pwrSensor.LimitFrequency = value |
Variable |
(Type) - Description |
|
pwrSensor |
A PowerSensorAsReceiver (Object) |
|
value |
(Boolean) - State of min and max frequency use. Choose from: False - Min and max frequencies disabled. True - Min and max frequencies enabled. |
Return Type |
Boolean |
Default |
False |
Examples |
pwrSensor.LimitFrequency = False 'Write limit = pwrSensor.LimitFrequency 'Read |
C++ Syntax |
HRESULT put_LimitFrequency(VARIANT_BOOL newVal); HRESULT get_LimitFrequency(VARIANT_BOOL* pVal); |
Interface |
IPowerSensorAsReceiver |