Write / Read
About Source Power Cal
About PMAR

Loss (Power Segment) Property


Description

Sets or returns the loss value associated with a PowerLossSegment.

VB Syntax

lossSeg.Loss = value

Variable

(Type) - Description

lossSeg

A PowerLossSegment (object)

A PowerLossSegmentPMAR (object)

value

(double) – Loss value in dB.  Loss is entered as a POSITIVE number.

Return Type

Double

Default

0

Examples

lossSeg.Loss = 0.5 'Write
lossVal = lossSeg.Loss 'Read

C++ Syntax

HRESULT put_Loss(Double newVal);

HRESULT get_Loss(Double *pVal);

Interface

IPowerLossSegment