Write/Read
About Magnitude Offset

MagnitudeOffset Property


Description

Offsets the data trace magnitude by the specified value.

To offset the data trace magnitude to a slope value that changes with frequency, use MagnitudeSlopeOffset Property.

To implement a Receiver Cal offset, use LogMagnitudeOffset property.

 VB Syntax

meas.MagnitudeOffset = value

Variable

(Type) - Description

meas

(object) - A Measurement object

value

(double)  - Offset value in dB.

Return Type

Double

Default

0

Examples

meas.MagnitudeOffset = 4 'Write

offs = meas.MagnitudeOffset 'Read

C++ Syntax

HRESULT put_MagnitudeOffset(double newVal);

HRESULT get_MagnitudeOffset(double *pVal);

Interface

IMeasurement4