Write/Read |
About Ext Pulse Gens |
Description |
Sets and returns the Master (On/Off) setting of the external pulse generator. this setting allows the external pulse generator to set the master clock frequency for the other pulse generators. |
VB Syntax |
extPulseGen.MasterMode = value |
Variable |
(Type) - Description |
|
extPulseGen |
An ExternalPulseGenerator (object) |
|
value |
(Boolean) Master setting. Choose from: True - Use the external pulse generator becomes the master clock frequency. False - Use the internal pulse generator as the master clock frequency. |
Return Type |
Boolean |
Default |
False |
Examples |
extPulseGen.MasterMode = True 'Write |
|
master = extPulseGen.MasterMode 'Read |
|
C++ Syntax |
HRESULT get_MasterMode (VARIANT BOOL *pValue) HRESULT put_MasterMode (VARIANT BOOL newVal) |
Interface |
IExternalPulseGenerator2 |
Last Modified:
|
15-Feb-2012 |
New topic |