Write/Read |
About iTMSA |
Description |
Sets and returns the stimulus mode for balanced measurements. |
VB Syntax |
balStim.Mode = value |
Variable |
(Type) - Description |
|
balStim |
A BalancedStimulus (object) |
|
value |
(Enum NABALSTIMulus) - Stimulus Mode. True modes are applicable only with Opt 460 - iTMSA. When a True-Mode is selected, the Balanced port powers are automatically uncoupled. Choose from: 0 - naSEStim: Single-Ended stimulus 1 - naTMStim: True-Mode stimulus 2 - naFTMStim: Forward only True-Mode stimulus 3 - naRTMStim: Reversed only True-Mode stimulus |
Return Type |
Enum |
Default |
0 - naSEStim: Single-Ended stimulus |
Examples |
balStim.Mode = naTMStim 'Write variable = balStim.Mode 'Read |
C++ Syntax |
HRESULT get_Mode(tagNABALSTIMulus *eVal ); HRESULT put_Mode(tagNABALSTIMulus eVal ); |
Interface |
IBalancedStimulus |