Read-only |
About E5091 Testset ControlAbout External Testset Control |
Description |
Returns the number of ports on the specified testset. Returns 0 if no test set is connected. |
VB Syntax |
value = tset.NumberOfPorts |
Variable |
(Type) - Description |
|
value |
(Long) variable to store the returned information. |
|
tset |
A TestsetControl object. OR An E5091Testset object. |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
value = testset1.NumberOfPorts |
C++ Syntax |
HRESULT get_NumberOfPorts(long *numberOfPorts); |
Interface |
ITestsetControl IE5091Testset |