Write/Read |
About Number of Points |
Description |
Sets or returns the Number of Points of the channel. Sets or returns the Number of Points of the segment. See Also
|
VB Syntax |
object.NumberOfPoints = value |
Variable |
(Type) - Description |
|
object |
Channel (object) or CalSet (object) - Read-only property |
|
value |
(long) - Number of Points. For channel, choose any number from 1 to the PNA max number of points. For segment, the total number of points in all segments cannot exceed the PNA maximum. A segment can have as few as 1 point. |
Return Type |
Long Integer |
Default |
201 for channel 21 for segment |
Examples |
chan.NumberOfPoints = 201 'sets the number of points for all measurements in the channel. -Write |
|
numofpts = chan.NumberOfPoints 'Read |
|
C++ Syntax |
HRESULT get_NumberOfPoints(long *pVal) |
Interface |
IChannel |CalSet3 |