Write/Read
About Receiver Attenuation

OffsetReceiverAttenuator Property


Description

Set and return whether to offset the reference receiver by the amount of receiver attenuation. Learn more.

This setting remains until changed or until the hard drive is changed or reformatted.

 VB Syntax

pref.OffsetReceiverAttenuator = value

Variable

(Type) - Description

pref

A Preferences (object)

value

(Boolean) - Choose from:

False Do NOT offset the test port receivers.

True  Offset the test port receivers.

Return Type

Boolean

Default

True  PNA-X models

False E836xB and PNA-L models

Examples

pref.OffsetReceiverAttenuator = 1 'Write

Rcvroffset = pref.OffsetReceiverAttenuator 'Read

C++ Syntax

HRESULT get_OffsetReceiverAttenuator(VARIANT_BOOL * val);

HRESULT put_OffsetReceiverAttenuator(VARIANT_BOOL val);

Interface

IPreferences6