Read-Write
About FOM

Offset Property


Description

Sets and returns the offset value to be used when coupling this range to the primary range.

This setting is valid only if the specified range is coupled to the primary range.

 VB Syntax

FOMRange.Offset = value

Variable

(Type) - Description

object

An FOMRange (object)

value

(Double) - Offset value.-(Unitless)

Return Type

Double

Default

0

Examples

fomRange.Offset = 1e9 'Write

Offs = fomRange.Offset 'Read

C++ Syntax

HRESULT get_Offset(double  *pVal)
HRESULT put_Offset(double  pVal)

Interface

IFOMRange