Read-only |
About Phase Control |
Description |
Returns the available phase control modes for the specified port. Use PhaseControlMode to set the Phase Control mode. |
VB Syntax |
phase.PhaseParameterModes(srcPort) = value |
Variable |
(Type) - Description |
|
phase |
A PhaseControl Object |
|
srcPort |
(Long Integer) Source port for which to make phase control settings. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(String) Choose from: "Off" - Turn phase control OFF "Openloop" - Sets a raw phase value for either swept phase or fixed phase, but no receivers are used to control the phase. "Parameter" - Sets and controls the phase of the signal at <port>. "Reference" - Reference port for a controlled (parameter) port. Use PhaseReferencePort to set the reference port. |
Return Type |
String |
Default |
"Off" |
|
Example |
value = phase.PhaseParameterModes 2' Read |
C++ Syntax |
HRESULT get_PhaseParameterModes(long port, BSTR* pVal); |
Interface |
IPhaseControl |
Last Modified:
|
8-Dec-2010 |
MX New topic |