Write/Read |
About Phase Sweep |
Description |
Sets and reads the state of phase sweep. Sweep type must be set to CWTime. |
VB Syntax |
balStim.PhaseSwpState = value |
Variable |
(Type) - Description |
|
balStim |
A BalancedStimulus (object) |
|
value |
(Boolean) State of phase sweep. False Phase sweep disabled. True Phase sweep enabled. |
Return Type |
Boolean |
Default |
False |
Examples |
balStim.PhaseSwpState = False 'Write var = balStim.PhaseSwpState 'Read |
C++ Syntax |
HRESULT get_PhaseSwpState (VARIANT_BOOL *bVal) HRESULT put_PhaseSwpState (VARIANT_BOOL bVal) |
Interface |
IBalancedStimulus2 |