Write / Read | 
About Port Extensions | 
Description | 
 Sets and returns the port extension delay in physical length (distance).  | 
VB Syntax | 
 fixture.PortDistance (port)= value  | 
Variable | 
(Type) - Description | 
| 
 fixture  | 
 A Fixturing Object  | 
| 
 port  | 
 (Integer) Port Number that will receive the delay setting.  | 
| 
 value  | 
 (Double) Physical length in distance. First specify units with PortDistanceUnit.  | 
Return Type | 
 Double  | 
Default | 
 0  | 
Examples | 
 fixture.PortDistance(2)= .01 'Write value = fixture.PortDistance(2) 'Read  | 
C++ Syntax | 
 HRESULT get_PortDistance(short portNum, double *pVal); HRESULT put_PortDistance(short portNum, double newVal);  | 
Interface | 
 IFixturing4  |