Write/Read
About GainCompressionCal
About SweptIMDCal

PowerLevel Property


Description

Set and read the power level at which to perform the Source Power Cal portion of a Gain Compression Calibration or a SweptIMD Cal.

 VB Syntax

object.PowerLevel = value

Variable

(Type) - Description

object

A GainCompressionCal (object)

A SweptIMDCal (object)

value

(Double) - Power level in dB. Choose a value from +30 to (-30). Learn about choosing a power level.

Return Type

Double

Default

0

Examples

gca.PowerLevel = -5 'Write

pLevel = imd.PowerLevel 'Read

C++ Syntax

HRESULT get_PowerLevel(double* pVal)

HRESULT put_PowerLevel(double newVal)

Interface

IGainCompressionCal

ISweptIMDCal