Write/Read |
About RF power during sweep retrace |
Description |
For single-band frequency or segment sweeps ONLY, specify whether to turn RF power ON or OFF during a retrace. This setting remains until changed using this command, or until the hard drive is changed or reformatted. |
VB Syntax |
pref.PowerOnDuringRetraceMode = value |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
value |
(Enum) - Choose from: 0 - naRetracePowerMode_Auto Power is left ON during retrace of single-band frequency or segment sweeps ONLY. 1 - naRetracePowerMode_OFF Power is turned OFF during retrace of single-band frequency or segment sweeps ONLY. |
Return Type |
Enum |
Default |
0 - naRetracePowerMode_Auto |
Examples |
pref.PowerOnDuringRetraceMode = naPowerSweepRetraceMode_Start 'Write |
|
psMode = pref.naPowerOnDuringRetraceMode_Start 'Read |
|
C++ Syntax |
HRESULT get_PowerOnDuringRetraceMode (tagNARetracePowerMode* preference); |
Interface |
IPreferences4 |
Last modified:
|
Nov. 16, 2006 |
New command |