Write/Read |
About Guided Power CalAbout NFXCal |
Description |
Set and read the cal kit to be used for calibrating at the reference plane when the power sensor connector is different from the DUT port. When used with Guided Power Cal, first enable a power cal using PerformPowerCalibration Property. |
VB Syntax |
object.PowerSensorCalkitType (n) = value |
Variable |
(Type) - Description |
object |
A GuidedCalibration (object) |
n |
(Long) PNA port number for which cal kit is specified. |
value |
(String) - Cal Kit. Use CompatibleCalKits Property to return a list of valid cal kits. |
Return Type |
String |
Default |
Not Applicable |
Examples |
gguided.PowerSensorCalkitType(1) = "85052B" 'Write |
ctype =guided.PowerSensorCalkitType(1) 'Read |
|
C++ Syntax |
HRESULT get_PowerSensorCalkitType(long port, BSTR* Val) HRESULT put_PowerSensorCalkitType(long port, BSTR newVal) |
Interface |
IGuidedCalibration6 |
Last Modified:
30-Nov-2010 |
Fixed example |
12-Oct-2009 |
MX New topic |