Write/Read |
About Receiver Leveling |
Description |
Sets and returns the safe mode power step value. |
VB Syntax |
RxLevel.PowerStep(srcPort) = value |
Variable |
(Type) - Description |
|
RxLevel |
A ReceiverLeveling Object |
|
srcPort |
(Long Integer) Source port for which to set the power step for Receiver Leveling. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(Double) Power step in dB. |
Return Type |
(Double) |
Default |
1 dB |
Examples |
rxLevel.PowerStep (1) = 2 ' Write |
|
value = rxLevel.PowerStep 2' Read |
|
C++ Syntax |
HRESULT get_PowerStep(long port, double* pVal); HRESULT put_PowerStep(long port, double newVal); |
Interface |
IReceiverLevelingConfiguration |
Last Modified:
|
13-Feb-2009 |
MX New topic |