Write/Read |
About Triggering |
Description |
Set and read the preference for the trigger behavior when performing an Unguided calibration. |
VB Syntax |
pref.PreferInternalTriggerOnUnguidedCal = bool |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
bool |
(Boolean) - Choose from: 0 - False - The trigger behavior during an Unguided calibration DOES respect the setting of the Trigger source command. For example, during an Unguided Cal, when Trigger source = External, the PNA will wait for the External trigger signal and then allow only one sweep. 1 - True -The trigger behavior during an Unguided calibration does NOT respect the Trigger Source = External setting. For example, during an Unguided Cal, when Trigger source = External, the PNA immediately switches to Internal sweep, measures the standard with one trigger signal, then switches back to External trigger. Note: When Trigger Source = Manual during a calibration, the PNA ALWAYS switches to Internal for one trigger to measure a standard, then back to Manual, regardless of this preference command. |
Return Type |
Boolean |
Default |
0 - False |
Examples |
pref.PreferInternalTriggerOnUnguidedCal = False 'Write |
|
prefer = pref.PreferInternalTriggerOnUnguidedCal 'Read |
|
C++ Syntax |
HRESULT put_PreferInternalTriggerOnUnguidedCal( VARIANT_BOOL bprefUnguided) HRESULT get_PreferInternalTriggerOnUnguidedCal( VARIANT_BOOL *bprefUnguided) |
Interface |
IPreferences2 |