Write/Read. |
About External Trigger |
Description |
Specifies the polarity of Ready for Trigger output. All existing Ready for Trigger outputs for PNA-X and PNA-L models are configured simultaneously with this command. See Capabilities Summary. The Ready for Trigger polarity can NOT be configured for E836x models. |
VB Syntax |
trigsetup.ReadyForTriggerPolarity = value |
Variable |
(Type) - Description |
|
trigsetup |
A TriggerSetup (object) |
|
value |
(Enum as NALevel) Choose from: 0 - naLow - Outputs a TTL low when the PNA is ready for trigger. 1 - naHigh - Outputs a TTL high when the PNA is ready for trigger. |
Return Type |
Enum |
Default |
0 - naLow |
Examples |
trigsetup.ReadyForTriggerPolarity = naLow 'Write |
|
pol = trigsetup.ReadyForTriggerPolarity 'Read |
|
C++ Syntax |
HRESULT get_ReadyForTriggerPolarity(tagNALevel *pVal); HRESULT put_ReadyForTriggerPolarity(tagNALevel newVal); |
Interface |
ITriggerSetup3 |