Read-only

ReceivePort Property


Description

Returns the receiver (response) port number of measurement. To understand how this property is useful, see IMeasurement2 Interface.

Note: Returning a receiver port is only supported for S-Parameter measurements.  If the measurement is not an S-Parameter, then E_NA_BAD_PARAMETER is returned.

 VB Syntax

value = meas.ReceivePort

Variable

(Type) - Description

value

(Long) - Variable to store the returned value

meas

A Measurement (object)

Return Type

Long Integer

Default

Not Applicable

Examples

rp = meas.ReceivePort

C++ Syntax

HRESULT ReceivePort(Long* rcvPort);

Interface

IMeasurement2