Write/Read |
About Receiver Attenuation |
Description |
Sets or returns the value of the specified receiver attenuator control. |
VB Syntax |
object.ReceiverAttenuator(rec) = value |
Variable |
(Type) - Description |
|
object |
Channel (object) or CalSet (object) - Read-only property |
|
rec |
(long integer) - Receiver with attenuator control to be changed. Choose from any of the available receivers in your PNA 1 - Receiver A 2 - Receiver B Receiver attenuation can not be set using logical receiver notation. |
|
value |
(double) - Attenuator value in dB. Choose any Long Integer between 0 and 35 in 5dB steps: If an invalid value is entered, the analyzer will select the next lower valid value. For example, if 19.9 is entered the analyzer will select 15 dB attenuation. |
Return Type |
Double |
Default |
0 db |
Examples |
chan.ReceiverAttenuator(1) = 5 'Write |
|
attn = chan.ReceiverAttenuator(2) 'Read |
|
C++ Syntax |
HRESULT get_ReceiverAttenuator(long lport, double *pVal) |
Interface |
IChannel |CalSet3 |