Write/Read
About Reference Position

ReferencePosition Property


Description

Sets or returns the Reference Position of the active trace.

 VB Syntax

trce.ReferencePosition = value

Variable

(Type) - Description

trce

A Trace (object)

value

(double) - Reference position on the screen measured in horizontal graticules from the bottom of the screen. Choose from any number between: 0 and 10.

Return Type

Double

Default

0

Examples

meas.ReferencePosition = 5 'Middle of the screen -Write

rpos = meas.ReferencePosition -Read

C++ Syntax

HRESULT get_ReferencePosition(double *pVal)
HRESULT put_ReferencePosition(double newVal)

Interface

ITrace