Write/Read |
About IM Spectrum |
Description |
Sets and returns the Resolution Bandwidth for the IM Spectrum measurement. |
VB Syntax |
ims.ResolutionBW = value |
Variable |
(Type) - Description |
|
ims |
An IMSpectrum Object |
|
value |
(Double) Resolution BW in Hz. Choose from: 60k | 100k | 150k | 300k, 600k | 1.0M | 3.0M If an invalid number is specified, the PNA will round up to the closest valid number. |
Return Type |
Double |
Default |
600 kHz |
Examples |
ims.ResolutionBW = 150e3 'Write |
|
value = ims.ResolutionBW 'Read |
|
C++ Syntax |
HRESULT get_ResolutionBW(double *pVal) |
Interface |
IIMSpectrum |