Write/Read
About Balanced Measurements

SBalMeasurement Property


Description

Sets and returns the measurement for the Single-Ended - Balanced topology.

 VB Syntax

balMeas.SBalMeasurement  = value

Variable

(Type) - Description

balMeas

A BalancedMeasurement (object)

value

(String) - Single-ended - Balanced Measurement parameter. Not case-sensitive. Choose from:

 

Sss11

Ssd12

Ssc12

Sds21

Sdd22

Sdc22

Scs21

Scd22

Scc22

Imb

CMRR1

(Sds21/Scs21)

CMRR2

(Ssd12/Ssc12)

Return Type

Sss11

Default

Not Applicable

Examples

balMeas.SBalMeasurement  = "Ssd12" 'Write

variable = balMeas.SBalMeasurement   'Read

C++ Syntax

HRESULT get_SBalMeasurement(BSTR *pVal)

HRESULT put_SBalMeasurement(BSTR newVal)

Interface

IBalancedMeasurement